You are here: Using KAS Simulator > Main Window

Describing KAS Simulator Graphical User Interface

Windows Overview

Main window

KAS Simulator main window contains:

In addition, the workspace contains two tabs to display the Axis and the I/Os.

Figure 6-8: KAS Simulator Main Window

KAS Simulator log window

This Log window shows all log messages related to the KAS Simulator. Error and warning messages issued from the operating system, as well as Printf Function instructions, are also placed on this window.

Every log message includes the following:

 

Windows Overview

Menus Overview


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™